NOTICE

If the operand value for a type conversion operator is outside of the value range
of the target data type, then the result output depends on the processor type and
is therefore undefined. This is the case, for example, when a negative operand value
is converted from LREAL to the target data type UINT.
Information can be lost when converting from larger data types to smaller data types.
The operators convert an integer value into the specified data types and return this type-converted value. If the number to be converted exceeds the range limit, then the first bytes of the number are ignored.
-
Call syntax
-
Converting to a string
-
Examples