Installation of Automation BuilderPermalink

Preconditions

Administrator rights are required on the PC to install Automation Builder.

Before beginning check that you have a working internet connection.

If you have any problems with your internet connection or proxy authentication or firewall settings, then choose the offline installation and licensing.

In case of an update installation:

Create a project archive before upgrading Automation Builder. Project archives contain all project data, including data that is not stored with a *.project file, e.g. device description files for third party devices.

⮫ “Creation of an archive ”

Installation

  1. Go to ‎⮫ abb.com/automationbuilder to access the Automation Builder homepage.

  2. Click on “Downloads” and confirm download of the latest released “Automation Builder” software.

    To install an older “Automation Builder” version click on “Automation Builder  Automation Builder Downloads” and download the desired version.

  3. Open the downloaded installer and follow the instructions of the installation manager.

  4. Installation_V3

    Keep the default installation type “Premium Edition”, if available.

  5. Select software packages to be installed:

    Enable the check box “PLC - AC500 V3”.

  6. Click “Download and install” and follow the instructions of the setup.