SF_MutingParPermalink

This is the web edition of the original ‎⮫ AC500-S safety user manual, version 1.3.2. This web edition is provided for quick reference only. The original safety user manual must be used to meet functional safety application requirements.

Standards

Requirements

IEC 61496-1:2012

A.7 Muting

A.7.1.2 There shall be at least two independent hard-wired muting signal sources to initiate the function. It shall not be possible to initiate muting when the OSSDs are already in the OFF-state.

A.7.1.3 The mute function shall only be initiated by the correct sequence and/or timing of the mute signals. Should conflicting muting signals occur, the ESPE shall not allow a muted condition to occur.

A.7.1.4 There shall be at least two independent hard-wired muting signal sources to stop the function. The muting function shall stop when the first of these muting signals changes state. The deactivation of the muting function shall not rely only on the clearance of the ESPE.

A.7.1.5 The muting signals should be continuously present during muting. When the signals are not continuously present, an incorrect sequence and/or the expiration of a pre-set time limit shall cause either a lock-out condition or a restart interlock.

A.7.4 Indication: A mute status signal or indicator shall be provided (in some applications, an indication signal of muting is necessary.

IEC / TS 62046/Ed. 2:2008

5.5. General application requirements for muting

ISO 13849-1:2015

5.2.2 Manual reset function

ISO 12100:2010

6.2.11.4: Restart following power failure/spontaneous restart

SF_MutingPar

Muting is the intended suppression of the safety function. In this FB, parallel muting with four muting sensors is specified.

This is required, e.g., when transporting the material into the danger zone without causing the machine to stop. Muting is triggered by muting sensors. The use of two or four muting sensors and correct integration into the production sequence must ensure that no persons enter the danger zone while the light curtain is muted. Muting sensors can be proximity switches, photoelectric barriers, limit switches, etc. which do not have to be fail-safe. Active muting mode must be indicated by indicator lights.

There are sequential and parallel muting procedures. In this FB, parallel muting with four muting sensors was used; an explanation is provided below. The FB can be used in both directions, forward and backward. The muting should be enabled with the MutingEnable signal by the process control to avoid manipulation.

The FB input parameters include the signals of the four muting sensors (MutingSwitch11 .. MutingSwitch22), the OSSD signal from the AOPD device (S_AOPD_In) as well as three parameterizable times (DiscTime11_12, DiscTime21_22 and MaxMutingTime).

The S_StartReset input shall only be activated if it is ensured that no hazardous situation can occur when the PES is started.

Table 1095: FB name: SF_MutingPar

Name

Data type

Initial value

Description, parameter values

VAR_INPUT

Activate

BOOL

FALSE

⮫ Table 1057 “General input parameters”

S_AOPD_In

BOOL

FALSE

Variable.

OSSD signal from AOPD.

FALSE: Protection field interrupted.

TRUE: Protection field not interrupted.

MutingSwitch11

BOOL

FALSE

Variable.

Status of muting sensor 11.

FALSE: Muting sensor 11 not actuated.

TRUE: Workpiece actuates muting sensor 11.

MutingSwitch12

BOOL

FALSE

Variable.

Status of muting sensor 12.

FALSE: Muting sensor 12 not actuated.

TRUE: Workpiece actuates muting sensor 12.

MutingSwitch21

BOOL

FALSE

Variable.

Status of muting sensor 21.

FALSE: Muting sensor 21 not actuated.

TRUE: Workpiece actuates muting sensor 21.

MutingSwitch22

BOOL

FALSE

Variable.

Status of muting sensor 22.

FALSE: Muting sensor 22 not actuated.

TRUE: Workpiece actuates muting sensor 22.

MutingEnable

BOOL

FALSE

Variable or constant.

Command by the control system that enables the start of the muting function when needed by the machine cycle. After the start of the muting function, this signal can be switched off.

FALSE: Muting not enabled.

TRUE: Start of muting function enabled.

S_StartReset

BOOL

FALSE

⮫ Table 1057 “General input parameters”

Reset

BOOL

FALSE

⮫ Table 1057 “General input parameters”

DiscTime11_12

TIME

T#0s

Constant 0..4 s;

Maximum discrepancy time for MutingSwitch11 and MutingSwitch12.

DiscTime21_22

TIME

T#0s

Constant 0..4 s;

Maximum discrepancy time for MutingSwitch21 and MutingSwitch22.

MaxMutingTime

TIME

T#0s

Constant 0..120 min (application area specific);

Maximum time for complete muting sequence, timer started when first 2 muting sensors are actuated.

VAR_OUTPUT

Ready

BOOL

FALSE

⮫ Table 1058 “General output parameters”

S_AOPD_Out

BOOL

FALSE

Safety related output, indicates status of the muted guard.

FALSE: AOPD protection field interrupted and muting not active.

TRUE: AOPD protection field not interrupted or muting active.

S_MutingActive

BOOL

FALSE

Indicates status of muting process.

FALSE: Muting not active.

TRUE: Muting active.

SafetyDemand

BOOL

FALSE

Optional.

⮫ Table 1058 “General output parameters”

ResetRequest

BOOL

FALSE

Optional.

⮫ Table 1058 “General output parameters”

Error

BOOL

FALSE

⮫ Table 1058 “General output parameters”

DiagCode

WORD

16#0000

⮫ Table 1058 “General output parameters”

Example for SF_MutingPar in forward direction with four sensors

1

04.06.112_MutingPar-1

If the muting sensors MutingSwitch11 (MS_11) and MutingSwitch12 (MS_12) are activated by the product within the time DiscTime11_12, muting mode is activated (S_MutingActive = TRUE).

The MaxMutingTime starts with the first actuated muting sensor.

2

04.06.113_MutingPar-2

Muting mode remains active as long as MutingSwitch11 (MS_11) and MutingSwitch12 (MS_12) are activated by the product. The product may pass through the light curtain without causing a machine stop.

3

04.06.114_MutingPar-3

Before muting sensors MutingSwitch11 (MS_11) and MutingSwitch12 (MS_12) are disabled, muting sensors MutingSwitch21 (MS_21) and MutingSwitch22 (MS_22) must be activated. This ensures that muting mode remains active. The time discrepancy between switching of MutingSwitch21 and MutingSwitch22 is monitored by the time DiscTime21_22.

4

04.06.115_MutingPar-4

Muting mode is terminated if either muting sensor MutingSwitch21 (MS_21) or MutingSwitch22 (MS_22) is disabled by the product. The maximum time for muting mode to be active is the MaxMutingTime.

Muting conditions

Forward direction

Muting condition 1 (to 8010) (MS_11 is the first entry switch actuated). Start timers MaxMutingTime and DiscTime11_12: MutingEnable AND (R_TRIG at MS_11 AND NOT MS_12 AND NOT MS_21 AND NOT MS_22)

Muting condition 1 (to 8310) (MS_12 is the first entry switch actuated). Start timers MaxMutingTime and DiscTime11_12: MutingEnable AND (NOT MS_11 AND R_TRIG at MS_12 AND NOT MS_21 AND NOT MS_22)

Muting condition 2 (from 8010) (MS_12 is the second entry switch actuated). Stop timer DiscTime11_12:

MutingEnable AND (MS_11 AND R_TRIG at MS_12 AND NOT MS_21 AND NOT MS_22)

Muting condition 2 (from 8310) (MS_11 is the second entry switch actuated). Stop timer DiscTime11_12:

MutingEnable AND (R_TRIG at MS_11 AND MS_12 AND NOT MS_21 AND NOT MS_22)

Muting condition 3 (both entry switches actuated in same cycle). Start timer MaxMutingTime:

MutingEnable AND (R_TRIG at MS_11 AND R_TRIG at MS_12 AND NOT MS_21 AND NOT MS_22)

Muting condition 4 (all switches actuated): MS_11 AND MS_12 AND MS_21 AND MS_22

Muting condition 24 (to 8030) (MS_21 is the first exit switch actuated). Start timer DiscTime21_22: MS_11 AND MS_12 AND R_TRIG at MS_21 AND NOT MS_22

Muting condition 24 (to 8330) (MS_22 is the first exit switch actuated). Start timer DiscTime21_22: MS_11 AND MS_12 AND NOT MS_21 AND R_TRIG at MS_22

Muting condition 25 (from 8030) (MS_22 is the second exit switch actuated). Stop timer DiscTime21_22: MS_11 AND MS_12 AND MS_21 AND R_TRIG at MS_22

Muting condition 25 (from 8330) (MS_21 is the second exit switch actuated). Stop timer DiscTime21_22: MS_11 AND MS_12 AND R_TRIG at MS_21 AND MS_22

Muting condition 5 (one of the exit switches released). Stop timer MaxMutingTime: NOT MS_11 AND NOT MS_12 AND (F_TRIG at MS_21 OR F_TRIG at MS_22)

Backward direction

Muting condition 11 (to 8110) (MS_21 is the first entry switch actuated). Start timers MaxMutingTime and DiscTime21_22: MutingEnable AND (NOT MS_22 AND R_TRIG at MS_21 AND NOT MS_11 AND NOT MS_12)

Muting condition 11 (to 8410) (MS_22 is the first entry switch actuated). Start timers MaxMutingTime and DiscTime21_22: MutingEnable AND (R_TRIG at MS_22 AND NOT MS_21 AND NOT MS_11 AND NOT MS_12)

Muting condition 12 (from 8110) (MS_22 is the second entry switch actuated). Stop timer DiscTime21_22:

MutingEnable AND (MS_21 AND R_TRIG at MS_22 AND NOT MS_11 AND NOT MS_12)

Muting condition 12 (from 8410) (MS_21 is the second entry switch actuated) . Stop timer DiscTime21_22:

MutingEnable AND (R_TRIG at MS_21 AND MS_22 AND NOT MS_11 AND NOT MS_12)

Muting condition 13 (both entry switches actuated in same cycle). Start timer MaxMutingTime:

MutingEnable AND (R_TRIG at MS_21 AND R_TRIG at MS_22 AND NOT MS_11 AND NOT MS_12)

Muting condition 14 (all switches actuated): MS_11 AND MS_12 AND MS_21 AND MS_22

Muting condition 44 (to 8130) (MS_11 is the first exit switch actuated). Start timer DiscTime11_12: MS_21 AND MS_22 AND R_TRIG at MS_11 AND NOT MS_12

Muting condition 44 (to 8430) (MS_12 is the first exit switch actuated). Start timer DiscTime11_12: MS_21 AND MS_22 AND NOT MS_11 AND R_TRIG at MS_12

Muting condition 45 (from 8130) (MS_12 is the second exit switch actuated). Stop timer DiscTime11_12: MS_21 AND MS_22 AND MS_11 AND R_TRIG at MS_12

Muting condition 45 (from 8430) (MS_11 is the second exit switch actuated). Stop timer DiscTime11_12: MS_21 AND MS_22 AND R_TRIG at MS_11 AND MS_12

Muting condition 15 (one of the exit switches released). Stop timer MaxMutingTime: NOT MS_21 AND NOT MS_22 AND (F_TRIG at MS_11 OR F_TRIG at MS_12)

Wrong muting sequences:

State 8000

(MutingEnable = FALSE when muting sequence starts) OR

((MS_11 OR MS_12) AND (MS_21 OR MS_22)) OR

(R_TRIG at MS_11 AND MS_12 AND NOT R_TRIG at MS_12) OR

(R_TRIG at MS_12 AND MS_11 AND NOT R_TRIG at MS_11) OR

(R_TRIG at MS_21 AND MS_22 AND NOT R_TRIG at MS_22) OR

(R_TRIG at MS_22 AND MS_21 AND NOT R_TRIG at MS_21) OR

((MS_11 AND NOT R_TRIG at MS_11) AND (MS_12 AND NOT R_TRIG at MS_12)) OR

((MS_21 AND NOT R_TRIG at MS_21) AND (MS_22 AND NOT R_TRIG at MS_22))

State 8010

NOT MutingEnable OR NOT MS_11 OR MS_21 OR MS_22

State 8310

NOT MutingEnable OR NOT MS_12 OR MS_21 OR MS_22

State 8020

NOT MS_11 OR NOT MS_12

State 8040

R_TRIG at MS_11 OR R_TRIG at MS_12 OR R_TRIG at MS_21 OR R_TRIG at MS_22

OR ((MS_11 OR MS_12) AND (F_TRIG at MS_21 OR F_TRIG at MS_22)) OR ((F_TRIG at MS_11 OR F_TRIG at MS_12) AND (F_TRIG at MS_21 OR F_TRIG at MS_22))

State 8030

NOT MS_11 OR NOT MS_12 OR NOT MS_21

State 8330

NOT MS_11 OR NOT MS_12 OR NOT MS_22

State 8110

NOT MutingEnable OR MS_11 OR MS_12 OR NOT MS_21

State 8410

NOT MutingEnable OR MS_11 OR MS_12 OR NOT MS_22

State 8120

NOT MS_21 OR NOT MS_22

State 8140

R_TRIG at MS_11 OR R_TRIG at MS_12 OR R_TRIG at MS_21 OR R_TRIG at MS_22

OR ((MS_21 OR MS_22) AND (F_TRIG at MS_11 OR F_TRIG at MS_12)) OR ((F_TRIG at MS_11 OR F_TRIG at MS_12) AND (F_TRIG at MS_21 OR F_TRIG at MS_22))

State 8130

NOT MS_21 OR NOT MS_22 OR NOT MS_11

State 8430

NOT MS_21 OR NOT MS_22 OR NOT MS_12

Typical timing diagram

Fig. 496: Typical timing diagram for SF_MutingPar

SF_MutingPar_TimingDiagram

Error detection

The FB detects the following error conditions:

  • DiscTime11_12 and DiscTime21_22 have been set to values less than T#0s or greater than T#4s.

  • MaxMutingTime has been set to a value less than T#0s or greater than T#120min.

  • The discrepancy time for the MutingSwitch11/MutingSwitch12 or MutingSwitch21/MutingSwitch22 sensor pairs has been exceeded.

  • The muting function (S_MutingActive = TRUE) exceeds the maximum muting time MaxMutingTime.

  • Muting sensors MutingSwitch11, MutingSwitch12, MutingSwitch21, and MutingSwitch22 are activated in the wrong order.

  • Muting sequence starts without being enabled by MutingEnable.

  • A static Reset condition is detected in states 8401 and 8402.

Error behavior

In the event of an error, the S_AOPD_Out and S_MutingActive outputs are set to FALSE. The DiagCode output indicates the relevant error code and the Error output is set to TRUE.

A restart is inhibited until the error conditions are cleared and the safe state is acknowledged with Reset by the operator.

Function block-specific error and status codes

Table 1096: FB-specific error codes

DiagCode

State name

State description and output setting

C001

Reset Error 1

Static Reset condition detected after FB activation in state 8401.

Ready = TRUE

S_AOPD_Out = FALSE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

C011

Reset Error 2

Static Reset condition detected in state 8402.

Ready = TRUE

S_AOPD_Out = FALSE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

CYx4

Error Muting sequence

Error detected in muting sequence state 8000, 8010, 8310, 8020, 8040, 8030, 8330, 8110, 8410, 8120, 8140, 8130 or 8430.

Ready = TRUE

S_AOPD_Out = FALSE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

Y = Status in the sequence (6 states for forward and 6 states for backward direction).

C0x4 = Error occurred in state 8000

C1x4 = Error occurred in state Forward 8010

C2x4 = Error occurred in state Forward 8310

C3x4 = Error occurred in state Forward 8020

C4x4 = Error occurred in state Forward 8030

C5x4 = Error occurred in state Forward 8330

C6x4 = Error occurred in state Forward 8040

C7x4 = Error occurred in state Backward 8110

C8x4 = Error occurred in state Backward 8410

C9x4 = Error occurred in state Backward 8120

CAx4 = Error occurred in state Backward 8130

CBx4 = Error occurred in state Backward 8430

CCx4 = Error occurred in state Backward 8140

...

CFx4 = Muting enable missing

x = Status of the sensors when error occurred (4 bits: LSB = MS_11; MS_12; MS_21; MSB = MS_22).

C010

Parameter Error

DiscTime11_12, DiscTime21_22 or MaxMutingTime value out of range.

Ready = TRUE

S_AOPD_Out = FALSE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

C020

Error Timer MaxMuting

Timing error: Active muting time (when S_MutingActive = TRUE) exceeds MaxMutingTime.

Ready = TRUE

S_AOPD_Out = FALSE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

C030

Error Timer MS11_12

Timing error: Discrepancy time for switching MutingSwitch11 and MutingSwitch12 > DiscTime11_12.

Ready = TRUE

S_AOPD_Out = FALSE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

C040

Error Timer MS21_22

Timing error: Discrepancy time for switching MutingSwitch21 and MutingSwitch22 > DiscTime21_22.

Ready = TRUE

S_AOPD_Out = FALSE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = TRUE

Table 1097: FB-specific status codes (no error):

DiagCode

State name

State description and output setting

0000

Idle

The function block is not active (initial state).

Ready = FALSE

S_AOPD_Out = FALSE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8000

AOPD Free

Muting not active and no safety demand from AOPD. If timers from subsequent muting are still running, they are stopped.

Ready = TRUE

S_AOPD_Out = TRUE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8401

Init

Function block has been activated.

Ready = TRUE

S_AOPD_Out = FALSE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = TRUE

Error = FALSE

8802

Safety Demand AOPD

Safety demand detected by AOPD, muting not active.

Ready = TRUE

S_AOPD_Out = FALSE

S_MutingActive = FALSE

SafetyDemand = TRUE

ResetRequest = FALSE

Error = FALSE

8402

Wait for Reset

Safety demand or errors have been detected and are now cleared. Operator acknowledgment by Reset required.

Ready = TRUE

S_AOPD_Out = FALSE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = TRUE

Error = FALSE

8002

Safe

Safety function activated.

Ready = TRUE

S_AOPD_Out = FALSE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8010

Muting Forward Start 1

Muting forward sequence is in starting phase after rising trigger of MutingSwitch 11. Monitoring of DiscTime11_12 is activated. Monitoring of MaxMutingTime is activated.

Ready = TRUE

S_AOPD_Out = TRUE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8310

Muting Forward Start 2

Muting forward sequence is in starting phase after rising trigger of MutingSwitch 12. Monitoring of DiscTime11_12 is activated. Monitoring of MaxMutingTime is activated.

Ready = TRUE

S_AOPD_Out = TRUE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8020

Muting Forward Active 1

Muting forward sequence is active either:

  • After rising trigger of the second entry MutingSwitch 12 or 11 has been detected.

  • When both MutingSwitch 11 and 12 have been actuated in the same cycle.

Monitoring of DiscTime11_12 is stopped. Monitoring of MaxMutingTime is activated, when transition came directly from state 8000.

Ready = TRUE

S_AOPD_Out = TRUE

S_MutingActive = TRUE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8030

Muting Forward Step 1

Muting forward sequence is active. MutingSwitch21 is the first exit switch actuated. Monitoring of DiscTime21_22 is started.

Ready = TRUE

S_AOPD_Out = TRUE

S_MutingActive = TRUE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8330

Muting Forward Step 2

Muting forward sequence is active. MutingSwitch22 is the first exit switch actuated. Monitoring of DiscTime21_22 is started.

Ready = TRUE

S_AOPD_Out = TRUE

S_MutingActive = TRUE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8040

Muting Forward Active 2

Muting forward sequence is still active. Both MutingSwitch21 and 22 are actuated, the monitoring of DiscTime21_22 is stopped.

Ready = TRUE

S_AOPD_Out = TRUE

S_MutingActive = TRUE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8110

Muting Backward Start 1

Muting backward sequence is in starting phase after rising trigger of MutingSwitch21. Monitoring of DiscTime21_22 is activated. Monitoring of MaxMutingTime is activated.

Ready = TRUE

S_AOPD_Out = TRUE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8410

Muting Backward Start 2

Muting backward sequence is in starting phase after rising trigger of MutingSwitch22. Monitoring of DiscTime21_22 is activated. Monitoring of MaxMutingTime is activated.

Ready = TRUE

S_AOPD_Out = TRUE

S_MutingActive = FALSE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8120

Muting Backward Active 1

Muting backward sequence is active either:

  • After rising trigger of the second MutingSwitch 21 or 22 has been detected.

  • When both MutingSwitch 21 and 22 have been actuated in the same cycle.

Monitoring of DiscTime21_22 is stopped. Monitoring of MaxMutingTime is activated, when transition came directly from state 8000.

Ready = TRUE

S_AOPD_Out = TRUE

S_MutingActive = TRUE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8130

Muting Backward Step 1

Muting backward sequence is active. MutingSwitch11 is the first exit switch actuated. Monitoring of DiscTime11_12 is started.

Ready = TRUE

S_AOPD_Out = TRUE

S_MutingActive = TRUE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8430

Muting Backward Step 2

Muting backward sequence is active. MutingSwitch12 is the first exit switch actuated. Monitoring of DiscTime11_12 is started.

Ready = TRUE

S_AOPD_Out = TRUE

S_MutingActive = TRUE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE

8140

Muting Backward Active 2

Muting backward sequence is still active. Both exit switches MutingSwitch11 and 12 are actuated, the monitoring of DiscTime11_12 is stopped.

Ready = TRUE

S_AOPD_Out = TRUE

S_MutingActive = TRUE

SafetyDemand = FALSE

ResetRequest = FALSE

Error = FALSE