SF_RTS_INFOPermalink

This is the web edition of the original ‎⮫ AC500-S safety user manual, version 1.3.2. This web edition is provided for quick reference only. The original safety user manual must be used to meet functional safety application requirements.

04.06.068_SF_RTS_INFO

Display of the firmware version of the safety CPU

This function provides the firmware version of the safety CPU. The version is a binary coded decimal, e.g., 16#10 means version 1.0.

Table 1144: FUN name: SF_RTS_INFO

Name

Data type

Initial value

Description, parameter values

VAR_OUTPUT

SF_RTS_INFO

WORD

16#0000

Firmware version of the safety CPU.

The upper BYTE of the entry represents the main version; the lower BYTE represents the subversion of the runtime system.

Example: RTS_VERSION = 16#0110 ➔ V01.1.0

Call in ST

SF_RTS_INFO_Value := SF_RTS_INFO();