Valuation of expressionsPermalink

The evaluation of expression takes place by means of processing the operators according to certain binding rules. The operator with the strongest binding is processed first, then the operator with the next strongest binding, etc., until all operators have been processed.

Operators with equal binding strength are processed from left to right.

Table 1182: ST operators in the order of their binding strength

Operation

Symbol

Binding strength

Put in parentheses

(expression)

Strongest binding

Function call

Function name (parameter list)

Exponentiation

EXPT

Negate Building of complements

- NOT

Multiply Divide Modulo

* / MOD

Add Subtract

+ -

Compare

<,>,<=,>=

Equal to Not equal to

= <>

Boolean AND

AND

Boolean XOR

XOR

Boolean OR

OR

Weakest binding

Table 1183: Instructions in ST

Instruction type

Example

Assignment  

A:=B; CV := CV + 1; C:=SIN(X);

Calling a function block and use of the FB output

CMD_TMR(IN := %IX5, PT := 300); A:=CMD_TMR.Q

RETURN

RETURN;

IF

D:=B*B;

IF D<0.0 THEN

C:=A;

ELSIF D=0.0 THEN

C:=B;

ELSE

C:=D;

END_IF;

CASE

CASE INT1 OF 1:

BOOL1 := TRUE; 2:

BOOL2 := TRUE;

ELSE

BOOL1 := FALSE;

BOOL2 := FALSE;

END_CASE;

FOR

J:=101;

FOR I:=1 TO 100 BY 2 DO

IF ARR[I] = 70 THEN

J:=I; EXIT;

END_IF;

END_FOR;

WHILE

J:=1;

WHILE J<= 100 AND ARR[J] <> 70 DO

J:=J+2;

END_WHILE;

REPEAT

J:=-1;

REPEAT

J:=J+2;

UNTIL J= 101 OR ARR[J] = 70

END_REPEAT;

EXIT

EXIT;

Empty instruction

;