FunctionalityPermalink

This is the web edition of the original ‎⮫ AC500-S safety user manual, version 1.3.2. This web edition is provided for quick reference only. The original safety user manual must be used to meet functional safety application requirements.

SVT reads the IEC 61131 program objects from the safety project created with AC500-S Programming Tool and the description files for the safety devices in Automation Builder, verifies the data from both sources and creates the SVT checklist. The SVT checklist is a text file that you can open with any text editor and print out, if necessary. Refer to the SVT checklist examples in figures that follow.

The SVT checklist has several sections:

SVT verifies, for example:

  • The integrity of the global variables for I/O mapping for each safety device in the safety project.

  • The integrity of the mapped I/O variables versus the I/O structure description.

  • The checksum of the F-Parameter for each safety device.

  • The integrity of F-Parameters with F-Parameter description.

DANGER

DANGER
DANGER
DANGER

DANGER

DANGER

In addition to successfully passed automatic checks, you must successfully complete all of the manual checks in the SVT checklist.

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

Use SVT on the final Automation Builder project after which no further changes in the functional safety project part leading to a new boot project CRC are expected.

Project information section

The SVT checklist starts with a section that is used to manually verify information regarding the whole safety project.

Fig. 466: Example of a project information section of an SVT checklist

SVT_checklist-01 (SVT) (AC500-S)

1

Time stamp and version information

2

Result of the automatic consistency checks done by SVT

3

Reference to the safety project

4

Data checksum for the whole SVT checklist

5

List of the safety devices in the safety project

Safety device sections

After the project information section, the SVT checklist has individual sections for each safety device in the safety project. The content of each safety device section depends on the type of the safety device.

ABB safety devices

Fig. 467: Example of a safety device section for DX581-S safety I/O module

DX581_S-01 (SVT) (AC500-S)

1

Result of the automatic consistency checks done by SVT

2

Data checksum for the safety device section

3

Safety device type description

4

Input and output mapping list for the safety device

5

List of F-Parameters for the safety device

F-Devices on AC500-S safety CPUs

F-Devices on AC500-S safety CPUs SM560-S-FD-1 and SM560-S-FD-4 include also a section with information on the position of the safety device in the safety project in Automation Builder.

Fig. 468: Example of a safety device section for a F-Device on AC500-S safety CPUs

_12_Byte_In_Out_Safety-01 (SVT) (AC500-S)

1

Position of the safety device in the safety project in Automation Builder under all CM589-PNIO(-4) nodes

3rd party safety devices

3rd party safety device sections also have Module ID and information on the GSDML file in the SVT checklist.

Fig. 469: Example of a safety device section for a 3rd party safety device

SIO_02_02-01 (SVT) (AC500-S)

1

Module ID

2

Information on the GSDML file

Safety CPU section

In the same way as for the safety device sections, the safety CPU section includes information about the automatic checks, the data checksum and the manual checks for the safety CPU.

Fig. 470: Example of a safety device section for safety CPU

Safety_CPU-01

1

Result of the automatic consistency checks done by SVT

2

Data checksum for the safety CPU section

3

Parameter "PROFIsafe startup timeout" of the safety CPU

Libraries section

The libraries section includes a data checksum to indicate changes for the used safety libraries and the CRCs of the used safety libraries.

Fig. 471: Example of the libraries section

Libraries-01 (SVT) (AC500-S)

1

Data checksum for the safety libraries

2

Library CRCs

End of SVT checklist

After the libraries section, the SVT checklist ends with the line ‎End of SVT checklist‎ and, after that, optional fields like date, signature, etc.

Fig. 472: End of SVT checklist with optional fields

SVT_end_of_checklist-02