Switch functionality of Ethernet interfaces ETH1/ETH2Permalink

As of SystemFW 3.1.0, the Ethernet interfaces ETH1/ETH2 can be configured as an Ethernet switch.

The default setting is “Two separate interfaces”.

switch_functonality_cut

Changes to the PLC Boot parameter ETH1 / ETH2 mode become active after a PLC reboot.

Create and download a boot project before rebooting the PLC.

Parameter

Value

Description

ETH1 / ETH2 mode

Two separate interfaces

Two separate Ethernet interfaces ETH1 and ETH2

Switch functionality ETH1-ETH2

Switch between ETH1 and ETH2

If the switch functionality ETH1-ETH2 is active, only the Ethernet interface ETH1 is available.

⮫ “[CFG] - configuration”

Any protocols configured under Ethernet interface ETH2 must be deleted. Otherwise, a compile error is created.

The setting of ETH1 / ETH2 mode can be checked on LED display using the soft key <CFG>.

⮫ “[CFG] - configuration”