Dialog: Project Settings: Security Permalink

Symbol: _cds_icon_security.png

Function: The dialog is used to configure the project protection by a password, a dongle, or a certificate.

Call: “Project  Project Settings” command, “Security” category

NOTICE

NOTICE
NOTICE
NOTICE

NOTICE

NOTICE

If you lose the encryption password, then you can no longer open the project. You can also no longer restore it.

“No protection”

cds_icon_radiobutton_activated.png: The project file is not protected from unauthorized access and data manipulation.

Note: We strongly recommend that you use a security feature.

cds_icon_radiobutton_activated.png: The “Password”, “Dongle”, and “Certificates” options cannot be selected.

“Integrity check”

When you create a new project, this option is enabled by default.

cds_icon_radiobutton_activated.png: The project file is stored in a proprietary format and its integrity is checked each time the project is loaded. The file may be incompatible with older versions of the development system.

Note that the project file is not encrypted. To better protect your data, activate one of the encryption functions.

“Encryption”

cds_icon_radiobutton_activated.png: The “Password”, “Dongle”, and “Certificates” encryption functions can be selected.

“Password”

Entering, changing and confirming the encryption password

When you save the project with these settings, you have to specify the password later in order to open the project again, even if it is to be loaded as a library reference.

“Dongle”

Requirement: You have connected the CODESYS security key (dongle) to the computer.

“Add”: The “Add Registered Dongle” dialog opens.

“Registered dongles”

List box of the registered dongles

“Certificates”

Certificates are used to encrypt the contents of the open project file.

Requirement: The certificates for all users who share the project have to be installed in the local memory.

_cds_icon_cert_store_open.png: The “Certificate Selection” dialog opens.

Table 705: “Add Registered Dongle”

“Dongle”

List box of all connected dongles

“Refresh”

CODESYS refreshes the list box.

“Blink”

The LEDs of the selected dongle flash for two seconds (if it supports this function).

The dongle has to be connected to the computer when CODESYS loads the project, even if it is loaded as a library reference.

For more information, see: ⮫ “Protecting and Saving Projects ”, ⮫ “General information about write and access protection ”, ⮫ “Encryption with certificates ”, ⮫ “User management and password manager ”, ⮫ “Permission management ”, ⮫ “Filing, saving ”