All EtherCAT Master errors are also available in the IEC application. The function block instance of each EtherCAT Master provides a property for reading the last error as an enumeration.
For more information, see: ⮫ IoDrvEtherCAT.LastError and ⮫ ETC_LASTERROR
|
Problem |
Possible Solution |
|---|---|
|
EtherCAT Master with red triangle in device tree Logger message: |
No communication is possible between the PLC and the first device. More than 100 consecutive packets have not been received. Possible causes:
Possible solution:
|
|
Some devices may have a red triangle in the device tree. Logger message: |
If sync unit groups are used and at least one device in the sync unit group is not operating correctly, the entire group is indicated as faulty. Not all EtherCAT Slaves transmit process data as expected. Input or output data may be missing. Possible causes:
Possible solution:
|
|
Some devices may have a red triangle in the device tree. Logger message: |
One or more devices are not communicating as expected. The inputs are not transmitted or the outputs are not used. Possible causes:
Possible solution:
|
|
Logger message: |
When "Distributed Clock" is used, the time of the first EtherCAT device with “Distributed Clock” enabled is used to synchronize the other devices and the PLC. This error message is displayed when the time value does not change. Possible causes:
Possible solution:
|
|
EtherCAT Master with red triangle in device tree Logger message: |
When the EtherCAT devices are started, the number of available devices is determined and the EEPROM of all devices is read. If no devices sre detected, this message is displayed. Possible causes:
Possible solution:
|
|
Logger message: |
The PLC runtime system could not transfer an EtherCAT packet. Possible causes:
Possible solution:
|
|
Logger message: |
The device detects an error and reports various error causes. Possible causes:
Possible solution:
|