To create an application program which can be run on the controller, you fill POUs with declarations and implementation code (source code), establish the link from the controller I/Os to application variables, and configure the task assignment. After checking and debugging, the CODESYS compiler creates the application code which can be downloaded to the controller.
The programming of the application POUs is supported by the programming language editors and other features such as text lists, image collections, alarm configurations, pragmas, refactoring, and ready-to-use POUs from CODESYS Development System or libraries.
There are features for syntax checking and code analysis, for achieving data persistence, and for encrypting the application code which is downloaded to the controller.