Command: NegatePermalink

Symbol: SmartPaste: uuid-d0aed091-ff22-f792-e0a3-a5fc962e7827

Shortcut: Ctrl + N

Function: The command negates the following elements:

  • Input/output of a block

  • Jump

  • Return

  • Coil

  • Contact

  • Variable

Call: Ladder menu; context menu

Requirements: The element to be negated is selected.

Examples:

Negated input and negated output on one function block:

SmartPaste: uuid-32fd497a-d07f-a776-b1e2-9097efeeb27e

Negated contact:

SmartPaste: uuid-386600c8-dbdd-8df6-14f6-f234a14353c6

Negated coil:

SmartPaste: uuid-a96e2775-dd97-9c6a-bf51-3b64ac8f225a