Symbol: Set
, Reset
Function: The Set command provides the element selected in the editor with a Set modifier. The Reset command provides the element with a Reset modifier.
For example, you can use it to make a Coil ⮫ “Element: Coil” and a non-primary block output into a "set coil". The command is available only at a suitable position.
Call: Ladder menu, Set/Reset submenu; context menu
You can use the keyboard combination Ctrl + M to toggle between Set, Reset, and no modifier on the selected element.