Command 'Compare with revision'Permalink

Symbol: _svn_icon_compare

Function: This command opens the “Project log” dialog or “Log - <object> ” where the version history is displayed from the project or an object of the CODESYS project. Here you can select a revision. A tab opens and shows the result of the comparison of your working copy and the revision.

Call: Context menu: “SVN”

Requirement: The object is versioned and not conflicted.

Multiple tabs can be open at the same time with the comparison of different objects.

Comparison by object type

Comparison by object type

The comparison dialog makes use of the functionality of the CODESYS command “Project  Compare”. In this way, objects are compared according to their object type.