Function: This command opens the “Gateway” dialog where you can define a gateway channel and add it to the current device configuration.
Call: Menu bar: “Gateway” in the “Communication Settings” dialog of the device editor.
Dialog 'Gateway'
|
“Name” |
Name of the gateway. |
|
“Driver” |
Driver type from a drop-down list. |
|
Driver-specific settings, for example: IP address, port |
Editable after double-clicking the predefined value. A short description for each parameter is displayed in the lower part of the dialog. Note: You can also specify the address of a DNS domain. This has to begin with |
The dialog is also used for later editing of the gateway entries of your project.
See also