Symbol: 
Function: This command switches the display of the connection between two elements back and forth between a connecting line and the use of connection marks.
Call: Main menu “CFC”, context menu
Requirements: A CFC editor is active. A connection or a connection mark is selected.
If you have selected a connecting line, the command removes this line and adds a “Connection Mark - Source” at the output of one element and a “Connection Mark - Sink” at the input of the other. Both are given the same name by default, “C-<n>”, where n is a sequential number.
If you select a pair of connection marks, the command converts these marks into a connecting line.
See also