Symbol: 
Function: The command creates a control point on a connecting line.
Call: Context menu “Routing”
Requirements: A CFC editor is active. The cursor is over a connection.
The control point is created in the position on the connection at which the cursor is located when calling the command. The command corresponds to the “Control Point” element in the “Tools” window.
See also