Function: This command opens the “Edit Worksheet” dialog box in which you set the size of the worksheet.
Call: Main menu “CFC”
Requirements: A CFC editor is active.
Dialog box 'Edit worksheet'
|
“Use following dimensions” |
Here is where you set the size of the worksheet. Your change is only accepted if the size is sufficient for the existing program. |
|
“Adapt the dimensions automatically” |
Automatically adapts the size of the worksheet to the size of your program. |
|
“Move the working sheet origin relatively” |
Shifts the worksheet along the x or y axis. The input of negative numbers is permitted. |