Symbol: 
Function: This command cancels all manual changes to the connections in the program and re-establishes the original state.
Call: Main menu “CFC Routing”, context menu “Routing”
Requirements: A CFC editor is active.
CODESYS cannot automatically route connections that are fixed by control points. You must
remove the control points before executing the command. Use the “Remove Control Point” command to do this. Furthermore you must disconnect connections that have been changed
manually and are marked by the
icon. Use the “Disconnect Connection” command to do this.