Symbol:
, shortcut: [Ctrl] + [B]
Function: This command inserts a box that is available in the project at the end of the selected network.
Call: Main menu “FBD, LD, IL”, context menu
Requirements: The FBD, LD or IL editor is active. A network is selected, but no box is selected.
If you select this command the input assistant opens, where you can select the desired box.
See also