Function: This command opens a dialog box for importing objects from an XML file in PLCopen format.
Call: Menu “Project”
Requirement: A project is open.
Dialog box 'Import PLCopenXML'
The dialog box lists all objects from the PLCopen export file that CODESYS can import at this point.
|
“Currently selected target object” |
Object that is selected in the Device tree |
|
“Insertable items” |
Displays all objects of the export file that CODESYS can insert below the selected object. |
The PLCopenXML scheme does not permit VAR_GLOBAL and VAR_GLOBAL CONSTANT POUs to be in the same variable list. Therefore, if you wish to export both, the variables must first be divided into two separate variable lists.