Function: This command opens the “Import and Export Options” dialog. Here you can configure the export and import of selected settings of the
CODESYS options. The settings are saved to an XML file with the default extension (options.xml).
Call: Menu bar: “Tools”.
Dialog 'Import and Export Options'
|
“Export selected options” |
“Select options”: In the table, you can select the categories of options, either user-specific or machine-specific (computer), whose current settings are to be exported to the XML file. “File”: Path of the export file in the local file system. Example: Button |
|
“Import selected options” |
“File”: Path of the options export file whose contents are to be imported. Button After you click “OK” to close the dialog, the settings described in the file are applied to the project. |
See also
: Opens the default dialog to search for an existing file in the local file system,
or to create one. The