Symbol: 
Function: This command opens the dialog box “License Repository” for viewing information about the individual licenses.
Call: Main menu “Tools”
Requirements: CODESYS is in offline or online mode.
In the license repository, after entering the ticket number, you can obtain information about the licenses concerned from the central license server.
To do this you can paste the ticket number(s) from the clipboard or import it/them from a text file.
|
<List of the ticket IDs imported into the repository for components requiring licenses> |
|
|
“Licenses” |
If you select an entry in the list of tickets, the name and the status of the licensed component are displayed here.
In the right-hand part of the dialog box you will then receive then the following information about this license: |
|
“Name”: name of the product to be licensed “Item number”: item number in the license server. “Return allowed”: It is possible to have this license deactivated so that it can be re-activated on another system. “Can be activated”: you can have the license activated via the license manager. “Activation quantitiy”: number of activations that have taken place so far. “Activation date”: date of the current activation “Container serial ” “Firm codes” “Comment” |
|
“Import Tickets” |
The standard dialog box for browsing the local file system appears. If you open a text file containing one or more “tickets”, i.e. license numbers, these are imported into the repository. Alternatively you can also insert the numbers from the clipboard into the list. |
: License available and valid
: License found, but invalid
: License not found