Symbol: 
Function: In CODESYS V3.5 version earlier than SP11, the command opens the “Memory” view.
Call: Menu bar: “View Memory”.
As of SP11, the command provides the notice that you must install the CODESYS Memory Tools package (available in the CODESYS Store) in order to use the memory view. After installation, you can open the “Memory” view by clicking “View Show Memory View”.