Function: Like the command “Add Device”, this command opens the dialog box “Add Device” for the selection of a device object that is to be inserted in the device tree in the currently selected slot.
Call: Context menu of the slot of a device object in the device tree.
Requirement: The slot of a device object is selected in the device tree.
An empty slot is identified by the symbol
and the entry "<empty> (<empty>)". An occupied slot is given the symbol
and the name of the device.
In the case of an occupied slot, this command replaces the existing module with the new one.