Function: This command reads the configuration file IoConfig.par of the PLC and stores the values in the project. Such a file is created if the parameters
of the PLC have been changed by another device, for example via a visualization. Then
these parameters are changed only in the memory of the PLC, but not in the configuration
of the project.
Call: Context menu of the PLC device object
Requirement: You have made the command available using the dialog in “Tools Customize”.