Symbol
; keyboard shortcut: [Ctrl]+[H]
Symbol
, keyboard shortcut [Ctrl]+[Shift]+[H]
Function: These commands scan the project or parts of it for a specified character string and replaces it.
Call: Menu bar: “Edit Find Replace”
Requirement: The application is in online mode.
This command opens the “Replace” dialog where the search and replace character strings are specified and the search options are defined.
|
“Replace with” |
Input field for the new character string. |
|
“Replace” |
Each next found string is highlighted in the editor and replaced (step-by-step replace). |
|
“Replace all” |
All found strings are replaced at one time without them being displayed in the editors. |
|
“Leave changed objects open after "Replace all"” |
The editors of the found objects remain open. |
Replacement in referenced libraries is not possible.