Symbol: 
Function: The command causes an LED of a connected controller to blink. As a result, the hardware can be identified clearly.
Call: The command is not in any menu by default. You can add it to a menu by means of the “Tools Customize” dialog, in the “Online” command category.
Requirement: The controller supports this function and the connection parameters are configured correctly.