In the generic “Files” tab of the device editor, you can copy files to and from the local file system and the controller.
Requirement: The vendor has unlocked the tab. In the device tree, the connection to the controller is configured. The device is running.
-
Double-click the PLC device object in the device tree to open the device editor.
-
Click the “Files” tab.
-
In “Host” | “Location” on the left part of the view, set the path in the local file system where files will be copied to and from. Example:
D:\FileTransferWithPLC. If necessary, create a new directory by clicking the folder symbol (
). The files and directories are shown like in a file manager. Click the refresh symbol (
) to update the display. -
In “Runtime” on the right side of the view, set the required directory for the data transfer in the same way.
CODESYS shows the files on the controller.
-
Select the required files from the file system tree for the file transfer (multiple selection is possible). You can also select a directory for transferring all files in a folder.
-
Click the left and right arrow symbols (
,
) between the two parts of the view.CODESYS copies the selected files to the other file system immediately. If a file is not already available in the target directory, then it is created. If it is already available and not write-protected, then it is overwritten. Otherwise a message is shown.
See also