Symbol: 
Function: This dialog is for the configuration of the settings for editing and printing in the CFC editor.
Call: menu “Tools Options”, category “CFC Editor”
Tab 'General'
|
“Enable AutoConnect” |
|
Make sure that you do not create unwanted connections when moving elements.
Tab 'View'
|
“Display grid points” |
|
|
“Show box icon” |
Requirement: You have either created the link for a function block or a function in the object properties or loaded it via a library. |
|
“Edit Line Colors” |
Opens the “Edit Line Colors” dialog. There you can define the colors for the connecting lines depending on the applied data type. The lines are then displayed in these colors in offline and online mode.
|
|
“Font” |
Display of the font and button for changing the font. |
Tab 'Print'
|
Setting the “Layout Options” |
|
|
“Fit method” |
“Page” or “Poster” |
|
“Scale” |
Possible values: 20 % - 200 % |
Tab 'Monitoring'
|
Settings for displaying the monitoring fields |
|
|
“Number of displayed digits” |
Number of displayed digits for floating-point numbers in the monitoring field Example: value: 12.345; number of displayed digits: 3; display: 12.3 |
|
“String length” |
Maximum length of string variable values in the monitoring field |
: When you drag a CFC element into the editor area, unlinked pins which "touch" each
other are automatically linked.