Function: This dialog shows the devices of the open project in which there are new versions available.
Call: Main menu “Project Project Environment” (“Device Versions” tab)
This dialog opens automatically when you open a project that contains an outdated device.
|
Names of the outdated devices and their versions, as well as the current version and the planned action. |
|
|
“Action” |
Double-click in the field to select the required actions. |
|
“Check for updates when loading this project” |
|
|
“Set all to newest” |
CODESYS uses the latest library version. |
|
“OK” |
CODESYS executes the selected actions. |
: The check is performed when the project is opened.
: The check is performed one time only.