Function: This dialog displays the libraries of the opened project for which newer versions are available.
Call: Main menu “Project Project Environment”, tab “Library Version ”
This dialog opens automatically when you open a project containing outdated libraries.
|
The list shows the name of the outdated library with version, the currently available version and the planned action. |
|
|
“Action” |
Double-click inside the field to select the desired actions. |
|
“Check for updates when loading this project” |
|
|
“Set all to newest” |
CODESYS uses the newest available version of the library. |
|
“OK” |
CODESYS performs the selected action(s). |
: Checking takes place each time the project is opened.
: Checking takes place once only.