Function: In this dialog, you configure the build environment and the necessary data for the integration of the C development environment.
Call: Main menu “View”, context menu of the object “C Code Module”
Requirement: The object “C Code Module” is selected in the device tree.




NOTICE

The dialog in this form is valid only for CODESYS Control Win V3 and Visual Studio. For other environments, the dialog can look different or may not even be available at all.
|
“Visual Studio location” |
Installation path of Visual Studio on the hard disk You can also select the path with the input assistant or search for it with the magnifying glass. |
|
“Windows SDK location” |
Installation path of Windows SDK on the hard disk You can also select the path with the input assistant or search for it with the magnifying glass. |
|
“Temporary build folder Location” |
Path on the hard disk for the temporary build files |
See also