Function: The tab contains options for the monitoring of transitions in SFC.
Call: Select transition object, click “Properties”; menu bar: “View Properties”.
|
“Enable monitoring” |
|
|
“Monitoring using call” |
Note: When you activate this option, you have to consider possible side effects. These kinds of side effects can occur if additional operations are implemented in the transition. |
: An implicit variable is created for the transition, which is then always given the
current property value when the application calls the Transition method. The value
stored last in this variable is displayed in the monitoring.