In this tabbed page of the generic device editor, you can backup and restore the application-specific file on the PLC by saving and reading a zip archive.
Requirement: The communication settings are correct for connection to the device. The application for backup is available on the PLC.
|
“Backup” |
This button opens a menu with the following commands:
|
|
“Restore” |
This button opens a menu with the following commands:
|
|
“ID” |
ID of the PLC (example: |
|
“Type” |
Device type (example: |
|
“Version” |
Device version (example: |
|
“File name” |
Storage path of the backup file. Clicking the symbol ( |
|
“Size of active files” |
(in kilobytes) Total size of the files set as active in the table (example: |
|
“Mode” |
Defines the scope of the backup: “Application”. The application-related files are added to the archive. |
|
“Comment” |
Optional entry for comments to be saved in the |
|
“Active” |
Required components are shown here with a green check mark (no check box). |
|
“Component” |
Affected components (example: |
|
“File” |
Name of the component file to back up (example: |
|
“Size” |
File size in bytes (example: |
|
“Requires STOP” |
|
See also

) opens the file system dialog box. Example:
: Optional files can be deactivated here for exclusion in the backup file.