This operator is an extension of the IEC 61131-3 standard.
The operator yields information about a variable. You can save the information as
data structure in a variable of data type __SYSTEM.VAR_INFO.
Syntax in the declaration:
<name of the info variable> : __SYSTEM.VAR_INFO; // Data structure for info variable
Syntax for the call:
<name of the info variable> := __VARINFO( <variable name> ); // Call of the operator
Example
FUNCTION_BLOCK FB_Velocity VAR_INPUT rVelocity: REAL := 1.2; END_VAR VAR_OUTPUT END_VAR VAR infoVelocity: __SYSTEM.VAR_INFO; //Info of Velocity END_VAR infoVelocity := __VARINFO(rVelocity); // Gets the info of Velocity locally
PROGRAM PLC_PRG VAR iCounter : INT := 0; // Counts the calls infoCounter : __SYSTEM.VAR_INFO; //Info of Counter arrA : ARRAY [1..2, 1..2, 1..2] OF INT := [0, 1, 2, 3, 4, 5, 6, 7]; // Stores the A data infoA : __SYSTEM.VAR_INFO; //Info of A fbVel : FB_Velocity; END_VAR iCounter := iCounter + 1; infoCounter := __VARINFO(iCounter); infoA := __VARINFO(arrA); fbVel();
The iCounter and arrA variables are recognized in the application code. The variable information is saved
in the infoCounter and infoA variables. Moreover, the FB_Velocity function block is instantiated.
Data type __SYSTEM.VAR_INFO
|
Name |
Data type |
Initialization |
Description |
|---|---|---|---|
|
|
|
0 |
Address of the variable Example: Note: For bit access of a variable |
|
|
|
0 |
Offset of the variable address (in bytes). Example: Note: If the variable is global, then the offset is relative to the beginning of the area. If the variable is a local variable in a function or method, then the offset is relative to the current stack frame. If the variable is a local variable in a function block, then the offset is relative to the function block instance. |
|
|
|
0 |
Memory area number Example: Note: The memory areas are device-dependent. |
|
|
|
0 |
Number of bits (in bytes) Example: Note: If the variable is not an integer data type, then: |
|
|
|
0 |
Memory size of the variable (in bits) Example: |
|
|
|
0 |
Bit address of the variable Requirement: The variable is located in the input memory area |
|
|
|
|
Data type class of the variable Example: Note: For user-defined data types or function block instances, |
|
|
|
'' |
Date type name of the variable as Note: For user-defined data types, the function block name or the DUT name is output. Example: |
|
|
|
0 |
Number of array elements Requirement: The variable has the data type Example: |
|
|
|
|
Elementary basic data type of the array elements. Requirement: The variable has the data type Example: |
|
|
|
0 |
Memory size of the array element (in bits) Requirement: The variable has the data type Example: |
|
|
|
|
Information about the memory area
Example: Note: The memory area configuration is device-dependent. |
|
|
|
'' |
Variable name as Example: |
|
|
|
'' |
Comment of the variable declaration Example: |