The effect of this pragma is that the components of an array used as an input variable for referenced visualizations are made visible in the Properties dialog box of the visualization.
Syntax:
{attribute 'ExpandFully'}
Insertion position: the line above the line with the declaration of the array.
Example
The visualization “visu” is to be inserted into a frame inside the visualization “visu_main”. arr is defined as an input variable in the interface editor of “visu” and will thus be available later for assignments in the Properties dialog box of
the frames in “visu_main”. In order to also make the individual components of arr available in this Properties dialog box, you must insert the attribute 'ExpandFully' directly before arr in the interface editor of visu. Declaration in the interface editor of “visu”:
VAR_INPUT
{attribute 'ExpandFully'}
arr : ARRAY[0..5] OF INT;
END_VAR