The attribute pragma is allowed for string variables and aliases. The attribute has the effect that the values of the variables are marked with it to be decoded in UTF-8 format during monitoring.
Syntax
{attribute 'monitoring_encoding' := 'UTF8'}
Example
PROGRAM PLC_PRG
VAR
{attribute 'monitoring.encoding' := 'UTF8'}
strDat : STRING := 'abc';
attribute 'monitoring_encoding' := 'UTF-8'}
strVarUtf8: STRING := UTF8#'你好,世界!ÜüÄäÖö';
{attribute 'monitoring_encoding' := 'UTF-8'}
str1: STRING := UTF8#'AÄyyy';
{attribute 'monitoring_encoding' := 'UTF-8'}
str2: STRING := UTF8#'AÄxxxÜÜÜ';
strVarUtf8_1: STRING := '你好,世界!ÜüÄäÖö';
str1_1: STRING := 'AÄyyy';
str2_1: STRING := 'AÄxxxÜÜÜ';
END_VAR