With the 'ProcessValue' attribute, you mark a component of a structure. In the CFC editor, you can then use
the command “Use attributed member as input” in order to connect this structure to an input of scalar type.
Syntax:
{attribute 'ProcessValue'}
Insert location: Line above the affected structure variable.
Example
TYPE QINT :
STRUCT
Status : STRING;
{attribute 'ProcessValue'}
Value1 : INT;
Value2 : INT;
END_STRUCT
END_TYPE