The JMP instruction is used to execute an unconditional jump to a program line that is marked
by a jump label.
Syntax:
<label>: <instructions> JMP <label>;
The jump label <label> is any unique identifier that you place at the beginning of a program line. On reaching
the JMP instruction, a return to the program line with the <label> takes place.
Example
iVar1 := 0; _label1: iVar1 := iVar1+1; (*instructions*) IF (iVar1 < 10) THEN JMP _label1; END_IF;




NOTICE

You must ensure by programming means that no endless loops are caused. For example, you can make the jump conditional.