Object: EtherCAT Slave
The tab provides slave status information and functions for the file transfer to the slave via EtherCAT (FoE).
Requirement: The expert settings for the slave are selected and the application is logged in to the controller.
|
“Init” |
Use for debugging purposes |
|
“Boot Strap” |
The slave is switched to Bootstrap Mode. Required if firmware files should be transferred to or from the slave |
|
“Pre-Op” |
Use for debugging purposes |
|
“Safe-Op” |
Use for debugging purposes |
|
“Op” |
Use for debugging purposes |
|
“Current status” |
|
|
“Requested status” |
|
“Port A” “Port B” “Port C” “Port D” |
Note: If the function is not supported, then the status can be hidden. |
|
“Download” |
Download of firmware files A dialog opens to save the firmware file. In this dialog, the input of a string as well as a password is necessary in order to execute the file transfer. The information should be taken from the data sheet of the slave. |
|
“Upload” |
Upload of firmware files A dialog opens to open the firmware file. In this dialog, the input of a string as well as a password is necessary in order to execute the file transfer. The information should be taken from the data sheet of the slave. |
|
“Write E²PROM” |
Writes the configuration of the slave to the E²PROM. A dialog for storing the configuration opens in the same way as for “File access over EtherCAT”. |
|
“Read E²PROM” |
Reads the configuration of the slave from the E²PROM. Upload of firmware files A dialog for opening the configuration opens in the same way as for “File access over EtherCAT”. |
|
“Write E²PROM XML” |
Writes the slave configuration directly from the XML file into the device. Can be executed only when configuration data exists in the XML file (<ConfigData> section). |