Object: EtherCAT Slave
The tab of the EtherCAT configurator displays the process data for the inputs and outputs of the slave. The data is preset from the device description file.
|
The table shows the outputs of the slave defined by “Start address”, “Type”, and “Index”. If outputs of the device are enabled here (for writing), then these outputs can be assigned to project variables in the “EtherCAT I/O Mapping” dialog. |
|
The table shows the inputs of the slave defined by “Name”, “Type”, and “Index”. If inputs of the device are enabled here (for reading), then these inputs can be assigned to project variables in the “EtherCAT I/O Mapping” dialog. |