Object: KNX
The I/O channels are generated for each communication object:
|
Signal |
Description |
|---|---|
|
“Program LED Status” |
This input is set by the ETS program. The signal can be used for identifying a special controller when several controllers are used (for example, by switching a LED). The status is also set when the “Program Button” is set to |
|
“Program Button” |
The “Program Button” is needed for assigning the physical address from ETS5. If the output is set to |
|
Signal |
Description |
|---|---|
|
“Status byte” |
Status byte as defined in the KNX stack. This allows you to determine in the application
whether or not data has been received. The status can be reset by means of the |
|
“Trigger/Disable Cyclic, send on change” “Trigger Output” |
Depending on the configuration in the ETS program, this output has the following function:
|
|
“Value” |
Value for the input or outputs – depending on the corresponding communication object. |