Object: PROFINET IO Module
|
“ID number” |
Identification of the module (from the device description). |
|
“Slot number” |
Position of the I/O module below the I/O device, starting at "1" for the first module and incremented for each additional module. This results automatically from the current structure in the device tree. |
|
“Set All Default Values” |
CODESYS resets all settings to default values (see default value column) from the GSDML file. |
|
“Read All Values” |
CODESYS reads the current values from the device and updates them in the editor. |
|
“Write All Values” |
CODESYS writes the current values from the editor to the I/O module. Not all I/O modules support parameter updates in run mode. If not, then an error message is displayed. |
See also