Object: PROFINET IO Field Device
The tab displays the basic communication settings.
|
“Use remanent data” |
The IP settings and the station name of the file are used. Initially, the IP address
is |
|
“Use project parameters” |
When starting the device, the values defined in the project for IP configuration and station name are always used initially. |
|
“Station name” |
The name of the device in the network. Note: The station name and the IP settings can deviate from the (default) settings
configured in the project. They can be set by the controller in runtime mode and in
some cases stored persistently (this means when this is specified for the controller
in the |
|
“IP address” |
Initial IP settings Caution: This data can be modified by the PROFINET IO Controller. The remanent data is stored on the file system of the controller. After the controller is restarted, this stored data goes into effect. The settings here are then ignored. |
|
“Subnet mask” |
|
|
“Default gateway” |
In online mode, the station name and the IP settings are displayed “Status” tab.
See also