Function: This command opens the “Export Trace Configuration” dialog box.
Call: context menu (right-click) the upper node in the tree view of the trace configuration.
Requirement: The dialog box “Trace Configuration” is active and the name of the trace configuration is selected in the tree view (example:
Visu_Trace1).
Dialog box 'Export Trace Configuration'
This dialog is used for saving the trace configuration to a text file that can be read by the runtime system.
|
“File name” |
Name of text file to be created. |
|
“File type” |
“Trace file (*.trace)”: Format that the runtime system component |
See also