Symbol: 
Function: This dialog is used for configuring the display of library visualizations and visualizations in the POUs view in the visualization editor. In addition, it is used for configuring the tab “Visualization Manager” - “Settings” (group “Style Settings”).
Call: Menu bar: “Tools Options” “Visualization Styles” category.
These settings are not applied at visualization runtime. In runtime mode, only the settings of the visualization manager are available in the “Settings” tab.
See also
'Style Configuration for Libraries and Global Visualizations'
|
These settings are applied for library visualizations and for visualizations in the POUs view. |
|
|
“Use no visualization style” |
|
|
“Use the following visualization style” |
|
|
“Derive visualization style automatically” |
|
|
“Fallback if no visualization style could be derived ” |
Style from list box Fallback solution in the case that no visualization style can be derived . Example: On the display variant, the automatically derived style results in a poor display due to the device. |
'Style Selection'
|
The drop-down list of “Selected style” can be configured in the visualization manager (“Settings” tab, “Style settings” group). |
|
|
“Display all versions” |
|
'Style for New Visualization Managers'
|
“Last used: <style, version, vendor>” |
Style that is selected automatically when you add a new visualization application. Note: It is actually possible that a display variant is displayed another way depending on the device despite this setting. |
|
“Preset: <style, version, vendor>” |
List box of styles from the style repository. |
: Visualizations in the POUs view or from libraries behave as if no style had been
selected.
: All other styles of the repository, including the selected style, are listed for
selection, but only in the latest version. If newer versions are installed for the
selected style, then these are also listed.
: All installed styles in all installed versions are available for selection.