Symbol: 
Function: The dialog box enables the setting of the visualization profile.
Call: Menu “Project Project Settings”, category “Visualization Profile”
Requirement: A project is open.
|
“Specific profile” |
Profile that CODESYS uses in the project and that determines the visualization elements that are available in the project. The selection list contains all the profiles installed so far. |