Symbol:

Category: “Special Controls”
The element shows the contents of text files that are saved on the controller. Files can be encoded in ASCII or Unicode formats.
A visualization user can also edit the text.
Element properties
|
“Element name” |
Example: |
|
“Type of element” |
“Text Editor” |
Element property 'Position'
The position defines the location and size of the element in the visualization window. These are based on the Cartesian coordinate system. The origin is located at the upper left corner of the window. The positive horizontal x-axis runs to the right. The positive vertical y-axis runs downwards.
|
“X” |
X coordinate of the upper left corner of the element Specified in pixels. Example: |
|
“Y” |
Y coordinate of the upper left corner of the element Specified in pixels. Example: |
|
“Width” |
Specified in pixels. Example: |
|
“Height” |
Specified in pixels. Example: |
You can also change the values by dragging the box symbols (
) to other positions in the editor.
Element property 'Font'
|
“Font name” |
Non-proportional font used by the visualization to display the contents of the file Example: “Courier New” |
|
“Size” |
Font size Example: |
Element property 'Control variables'
|
“Variable” |
Variable ( Example: |
|
“Open” |
Variable ( Example:
|
|
“Close” |
Variable ( Example:
|
|
“Save” |
Variable ( Example:
|
|
“New” |
Variable ( Example:
|
|
“Variable” |
Variable ( Example: |
|
“Find” |
Variable ( Example:
|
|
“Find next” |
Variable ( Example:
|
|
“Line” |
Variable (integer data type). Contains the line of the cursor Example: |
|
“Column” |
Variable (integer data type). Contains the column of the cursor Example: |
|
“Position” |
Output variable (integer data type). Shows the absolute cursor position in the text. Example: |
|
“Set cursor” |
Variable ( Example:
Note: The variable is used as the control variable for an input event triggered by a visualization user. |
|
“Start position” |
Output variable (integer data type). Shows the absolute position for starting the text selection Example: |
|
“End position” |
Output variable (integer data type). Shows the absolute position for ending the text selection. Example: |
|
“Start line number” |
Output variable (integer data type). Shows the line where the text selection begins Example: |
|
“Start column index” |
Output variable (integer data type). Shows the column where the text selection begins Example: |
|
“End line number” |
Output variable (integer data type). Shows the line where the text selection ends Example: |
|
“End column index” |
Output variable (integer data type). Shows the column where the text selection ends Example: |
|
“Line to select” |
Variable (integer data type). Contains the line number that is selected Note: The selection is controlled by the variables in the “Trigger selection” property. |
|
“Set selection” |
Variable ( Example:
if the line is not in the current text segment of the Text Editor, then the text segment is moved to this line. Note: The variable is used as the control variable for an input event triggered by a visualization user. The control variable is not reset automatically. You are responsible for this to occur in the visualization. |
|
“Variable for error code” |
Variable (integer data type). Contains the error code when an error occurs Example: The error codes are declared in |
|
“Variable for content changed” |
Variable ( Example:
|
|
“Variable for access mode” |
Variable ( Example:
Note: The variable overwrites the setting in the “Editor mode” property. |
|
“Maximum line length” |
Maximum number of characters per line |
|
“Editor mode” |
|
Element property 'New files'
|
“Encoding” |
Character encoding of the new file:
|
|
“New line character sequence” |
End of line character of the new file:
Please note: When a visualization user opens an existing file, the end-of-line character of the file is detected and used automatically. |
These properties are available only when you have selected the “Support client animations and overlay of native elements” option in the Visualization Manager.
|
“Animation duration” |
Defines the duration (in milliseconds) in which the element runs an animation
Animatable properties
The animated movement is executed when at least one value of an animatable property has changed. The movement then executed is not jerky, but is smooth within the specified animation duration. The visualization element travels to the specified position while rotating dynamically. The transitions are smooth. |
|
“Move to foreground” |
Moves the visualization element to the foreground Variable ( Example:
|
Element property 'Access rights'
Requirement: User management is set up for the visualization.
|
“Access rights” |
Opens the “Access rights” dialog. There you can edit the access privileges for the element. Status messages:
|
See also