The pragma {attribute 'parameterstringof'} allows that the instance name of the specified parameter is made accessible for
the referenced visualization. An interface variable (STRING) will contain the instance name of the specified parameter. The interface variable
is visible within the referenced visualization and can for example be used in a text
output.
Syntax:
{attribute 'parameterstringof' := '<variable>'}
Example: declaration of a interface
VAR_INPUT
{attribute 'parameterstringof' := 'iftDut_A'}
sItfNameDut_A: STRING;
END_VAR
VAR_IN_OUT
iftDut_A : DUT_A;
END_VAR