Function: The dialog shows all device security settings which are provided by the connected controller.
Call: “Communication Settings” tab, “Device” → “Security Settings” menu command
Requirements: You have installed CODESYS Security Agent and the active path to the controller is configured.
The following table shows the settings which affect the OPC UA Server.
|
Setting |
Description |
|---|---|
|
|
Applied OPC UA security policy. The selected policy and all more secure options are used.
|
|
|
Mode for communication
|
|
|
Activation/Deactivation OPC UA Server
|
|
|
UserToken of the OPC UA Server
|
|
|
Transfer passwords in plain text if a OPC UA Server certificate is not available
|
|
|
Enable/Disable check of certificate revocation lists (CRLs). CRLs are used for CA-signed certificates.
For more information, see: |
|
|
The OPC UA specification requires that for self-signed certificates the
|
|
|
The OPC UA protocol requires mutual authentication of the applications when establishing
a connection.
This is achieved with safeguarded connections (signing or signing+encryption) by means
of the mutual
validation of the application certificates ( You can use the
|
|
|
Disabling of security policies Entry as a policy URL (for example |
|
|
Defines the |
|
|
Defines the |
|
|
Defines the |
|
|
Defines the |
|
|
Defines the |